Directive 2011/65/EU on the Restriction of the use of certain Hazardous Substances in Electrical and Electronic Equipment (RoHS)
RoHS came into force on 21 July 2011. It prohibits the marketing of new electrical and electronic equipment containing more than a specific level of certain hazardous substances. Substances that are subject to restrictions are listed in Annex II 2011/65/EU (% by weight): Lead (0.1%), Mercury (0.1%), Cadmium (0.01%), Hexavalent chromium (0.1%), Polybrominated biphenyls (PBB) (0.1%), and Polybrominated diphenyl ethers (PBDE) (0.1%). From 22 July 2019, Delegated Directive 2015/863/EU will come into force and extend the list of restricted substances to include: Bis(2-ethylhexyl) phthalate (DEHP) (0.1%), Butyl benzyl phthalate (BBP) (0.1%), Dibutyl phthalate (DBP) (0.1%), and Diisobutyl phthalate (DIBP) (0.1%). Medical devices and monitoring and control instruments are subject to a transition period until 22 July 2021.